1/20/2015 12:38 PM | |
Posts: 9 Rating: (0) |
Exactly, V13 UPD6 was working fine. I will try a new installation deleting first de complete directory. Thanks
|
1/20/2015 5:13 PM | |
Posts: 56 Rating: (1) |
Do you have V13 WinCC and/or V13 Safety installed? If so you must obtain and installthe SP1 for these packages as well. |
1/24/2015 9:55 PM | |
Posts: 15 Rating: (0) |
I have had the same experience. I am currently unsintalling and will attempt a install of V13 (non-SP1). |
9/14/2015 5:02 PM | |
Posts: 16 Rating: (0) |
Hello, I have the same problems here. So i tried to uninstall everything, delete the registry and then reinstall, but i still got some erros. (see the attachment) Can someone help me ? AttachmentSIA_STEP7_PRO_V13@15-09-14_11-48-03_summary.rar (490 Downloads) |
9/14/2015 6:28 PM | |
Posts: 16 Rating: (0) |
here it is. installing whitout the antivirus dont change anything ;( AttachmentSIA_STEP7_PRO_V13@15-09-14_12-18-28.rar (346 Downloads) |
9/14/2015 6:43 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011) |
Hi, it looks that there are any Registry Keys defect or not available. This can cause from a older installation. I think you should complete uninstall the TIA SW like described in the FAQ: https://support.industry.siemens.com/cs/ww/en/view/76325723 And then install it on the clean system
Christoph |
This contribution was helpful to1 thankful Users |
Follow us on