4/11/2017 7:36 AM | |
Joined: 10/5/2006 Last visit: 3/11/2025 Posts: 74 Rating:
|
The problem also exists in WinCC V14 SP1. I cannot use WinCC V14 if the symbolic I/O field does not function properly. I had to use V13 SP1 Upd9 (I did not upgrade to V13 SP2 yet). I've attached a video that shows the problem. When you see the Symbolic I/O field open and close right away, I am only left-clicking once on it. When you see the symbolic I/O field staying open, I am left-clicking on it, and while holding the left mouse button, I move the cursor over the scroll bar. Only then am I able to click on a value (a/b/c) to select the value I want. At no other time, does the Symbolic I/O field stay open. This is a bug that needs to be fixed by Siemens. PS: I am using WinCC Advanced RT V14 SP1 AttachmentTIAV14_Symbolic_IO_Problem.zip (567 Downloads) |
Last edited by: sdyson at: 4/11/2017 7:37:22 AMAutomation Programmer |
|
10/19/2023 10:31 AM | |
Joined: 8/3/2009 Last visit: 3/19/2025 Posts: 15020 Rating:
|
Hello Check out also this FAQ : https://support.industry.siemens.com/cs/de/en/view/109749354 It was created since my last Post to this Topic Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on