10/4/2018 4:06 AM | |
Joined: 7/5/2013 Last visit: 4/24/2025 Posts: 3148 Rating:
|
Hello Jeebs, in general I would not log directly to an archive in the network, because you have no logs when it is disconnected for any reason. Better create the logs on a local memory and copy resp. move them to the network when they are closed - see How do you safely copy and move archives with WinCC Comfort/WinCC Advanced? Anyway, logs have the property "Restart behaviour > Enable logging at runtime start". Deactivate it and e.g. check the point of runtime start in the PLC and set a tag after the required delay. On change of this tag call system function StartLogging. Regards, Frink |
Pi is exactly three! |
|
Follow us on