1/6/2023 5:09 PM | |
Joined: 11/22/2013 Last visit: 9/18/2023 Posts: 7 Rating:
|
Thank you for the detailed information. I have gone through the migration documentation. But I end up having problems, the TIA portal V15 doesn't compile the HMI at all and gives error. My_Scenario: Target-1: Upgrade the Protool program to TIA Portal. Target-2: Change the device type from Panel PC to Comfort Panel TP 1200/1500. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/09/2023 11:20:40New subject after splitting |
|
1/9/2023 11:22 AM | |
Joined: 5/12/2006 Last visit: 4/24/2025 Posts: 22624 Rating:
|
migrate the winccflex to tia if you get a eror please provide a screen of the errormessages. |
1/17/2023 11:01 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello EntrepreneurAlvi generally this should work. If you have the Runtime in TIA Portal you also can change the device to a Comfort panel. Here are some basic manuals for migration but they fits not 100% because of the Runtime. But should work as well: https://support.industry.siemens.com/cs/ww/en/view/18796902 https://support.industry.siemens.com/cs/ww/en/view/49752044 A suppose you have migrated the Runtime already to your TIA project, which error message do you get? bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on