7/11/2018 11:35 AM | |
Joined: 1/5/2011 Last visit: 6/15/2024 Posts: 815 Rating:
|
I have the same problem. Installed on my desktop without any problems, now I am trying to install it on my field pg M4 from siemens and it does not work! I have the same problem as AutoGen_7593493 . For some odd reason the installation skips General settings and configuration and goes straight to Install (overview/modify system/system configuration), when that finishes I am asked to reboot my computer to finish the installation. When my computer reboots it just start the installation again from scratch. I have tried the suggestion by userWizard, but I the PendingFileRenameOperations is not present in the registery, so there is no option adjust this parameter!!! I've ran the installation as administrator like suggested by userhuggy_d1, but that didn't seem to fix the problem either. I've already tried to delete the temp installation files, re-download and start from scratch, but that didn't work either. Someone from Siemens should look in to this problem ASAP and write a solution on their site. If anyone has suggestions (other than those that are already given and do not work), in the meanwhile. I would appreciate them very much. Thanks in advance. Jens |
Keep it simple and on-topic. |
|
7/11/2018 6:13 PM | |
Joined: 7/7/2010 Last visit: 7/17/2024 Posts: 14970 Rating:
|
What are the hardware specs of your M4? Do they meet the minimum requirements for TIA portal V15?
|
science guy |
|
8/14/2018 9:42 AM | |
Posts: 8 Rating:
|
Hello, does anybody solved that problem? I have the same issues like Jens_app. I use laptop HP with requirement HW, Win10 Pro 1803. Thanks. |
8/14/2018 10:22 AM | |
Posts: 8 Rating:
|
Which files are important? When I zip the folder, it has about 160MB. |
8/14/2018 10:32 AM | |
Joined: 5/12/2006 Last visit: 7/17/2024 Posts: 22317 Rating:
|
all files use dropbox or any other filehoster for the Upload. |
8/14/2018 10:46 AM | |
Posts: 8 Rating:
|
Here is my log folder: https://www.dropbox.com/s/grnlmsuv52tpa7y/AUTINSTLOG.zip?dl=0 |
Last edited by: ham_ax at: 8/14/2018 10:47:38 AM |
|
8/14/2018 2:15 PM | |
Posts: 8 Rating:
|
I installed SIMATIC STEP 7 and SIMATIC WinCC from installation DVD 1/2. I also tried download installation from this link, but the same problem. The installation begins and after couple minutes finished and wants restart. It does not create folder in C:\Program Files\Siemens\Automation\Portal V15 nor icon on the desktop... |
Last edited by: ham_ax at: 8/14/2018 2:16:19 PMLast edited by: Jen_Moderator at: 8/15/2018 8:40:49 AMOptimized link. |
|
Follow us on