3/23/2023 7:23 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello U_d524ebdf-2b05-4... Check this FAQ: https://support.industry.siemens.com/cs/de/en/view/109754931 --> I cannot believe that the V15..1 project has a Comfort Panel with a V12 image integrated. This is only possible up to TIa v14. The Image Version is too old. It has to be opened with the last version in which you have worked on it then change the Image Version of the HMi to the latest version and then you can also migrate to the newer TIA version. Bye Murof |
Last edited by: Murof at: 03/23/2023 07:24:12If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on