10/23/2015 8:50 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:51 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:52 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:52 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:53 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:53 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:53 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:54 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:54 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:55 PM | |
Posts: 24 Rating: (0) |
. |
10/23/2015 8:58 PM | |
Posts: 24 Rating: (0) |
. |
10/26/2015 3:41 PM | |
Posts: 24 Rating: (0) |
capraloris, thank you, I did what items 2 and 3 say but still not working. |
10/26/2015 4:53 PM | |
Posts: 24 Rating: (0) |
. |
10/26/2015 7:18 PM | |
Posts: 24 Rating: (0) |
... Then I tried with 'e1000e' and I can't ping the PLC. Figure 16. Best Regards. Freddye Delgado |
10/27/2015 12:43 PM | |
Posts: 24 Rating: (0) |
Dear Michael K, my method to change the netcard is shutdown the virtual machine, close down VMware and manually edit .vmx file on Notepad, setting for example: ethernet0.virtualDev = "e1000" or ethernet0.virtualDev = "vmxnet3" Then, when I run the virtual machine, the driver is automatically installed. See the attached .vmx file (as .txt) Best Regards, fredito AttachmentVM - TIA Portal 13 SP1 - copy.txt (450 Downloads) |
Last edited by: fredito at: 10/27/2015 12:49:41 PM |
|
10/28/2015 6:23 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
this is wrong! TIA V13 support and is released for Win7 32bit Operating System. You can check this with the compatibility tool! Regards Christoph AttachmentSTEP-7-Professional-(TIA-Portal)_V13.0_compatibility-list_en_2015-10-20.xlsx (284 Downloads) |
10/28/2015 1:55 PM | |
Posts: 24 Rating: (0) |
Yes, ChristophD, you are right, in fact:
Anyway, I'm now installing TIA Portal V13 SP1 on Windows 7 64-bits (Virtual Machine) Best Regards, fredito |
1/15/2016 9:00 AM | |
Posts: 15 Rating: (0) |
I would like to try NIC Vlance on win7 machine? It works for XP... But, I can't find drivers for AMD 79C970 PCnet32 LANCE for win7. Does it even exist? |
12/20/2016 9:32 AM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1645) |
Hello Jan Yes Connection with Wireless Lan ist always tricky because the WLAN Access points often do not forward the MAC Adress Broadcast Telegrams of the "accessable devices or something else" often you can only use a direct IP Connetion if the Access Point has no such Option to set. you say teh Ping to the Device you want to load or go online is OK and you can do also a Online Sight. At the Panel just look if the Transfer settings is Ethernet not PN/IE and in the Transfer Option in TIA Portal also use Ethernet (or PN/IE on both side) look to this FAQ: https://support.industry.siemens.com/cs/ww/en/view/88633853 Bye Murof |
If this Information really helps, you could use the Rate function |
|