8/30/2019 7:21 AM | |
Joined: 5/12/2006 Last visit: 4/24/2025 Posts: 22624 Rating:
|
Hello, yes it can be installed side by side to Step7 V5.6. You have two choices: 1. use Step7 V5.6 for PLC, and TIA for the HMI -> Device Proxy 2. migrate the complete project from Step7 V5.6 to TIA Portal -> check if this is possible with you used HW Do you would recreate the HMI from stratch? migrate the Protool Project to WinCC flexible 2008 (here you can use only up to 2008 SP2 for Migration) then migrate this project to TIA WinCC V14 (this is must because the older Panels from WinCCflex not supported in TIA V15.1) change the Panel type in WinCC V14 to the KP700 open this project in TIA V15.1 and Update the project/HMI Regards Christoph |
This contribution was helpful to
1 thankful Users |
Follow us on