11/25/2013 10:35 AM | |
Joined: 3/3/2012 Last visit: 10/24/2023 Posts: 11 Rating:
|
Hello I want to open http://support.automation.siemens.com/WW/view/en/57132240 STEP7_(TIA_Portal)_AT_KeyWord example,But it tell me to install TIA SP1,I download Tia sp1 but it didnot installed, Can evrerybody Convert the version of this program to V11 or V12 without SP1,that is i can open example only with TIA V12 professional and with no need to sp1,and then upload here? It is only 1_open the project 2_save as V11 Thanks |
Last edited by: O_Moderator at: 11/25/2013 12:58 PMlink corrected Last edited by: chelinaa at: 11/25/2013 12:17 PM |
|
Follow us on