3/21/2015 1:02 PM | |
Posts: 3 Rating: (0) |
Hi all,i'm using TIA Portal v12,i create a project with plc s7-1500 and KTP400 HMI.First everything works good,i can add new screen and edit them,but my problem now is when i click to open or add new screen i get alert message "the application has encountered a problem and needs to close" (restart/close).I tried to create new project but i get the same problem when i add HMI Panel.The simulation works good if i start HMI simulation but i can't open or create new screen. Help me please and thank you :) ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/23/2015 9:19:47 AMNew subject after splitting |
|
3/21/2015 4:12 PM | |
Posts: 5225 Rating: (1184) |
Get TIA12 updated as far possible.. there is a SP1but I'm not sure of the update version. Start at [LINK1] and [LINK2]. This forum had many interesting issues resolved when updating the software (TIA11 and TIA12). w |
Last edited by: William_B at: 3/21/2015 4:14:20 PMLast edited by: William_B at: 3/21/2015 4:16:22 PMSTEP7 and WINCC needs seperate updates! Give 2 links. |
|
This contribution was helpful to1 thankful Users |
Follow us on