2/10/2016 11:28 AM | |
Joined: 7/22/2013 Last visit: 1/20/2025 Posts: 8 Rating:
|
Hi, I am facing now an issue: When I start simulation of HMI (KTP400 BASIC PN generation2) and I am connected to PLC via VPN(TS ADAPTER), I cant see values on the simulated screen, only crosses (#). This has been working without problems till last week, for about 2-3 months, and I am not aware of any change in the TIA PORTAL. I am still running V13 SP1 update5. On my colleagues computer the values are still vissible. I can go online with PLC and check the vallues there, the connection via VPN is still working without problems. Setting PG/PC is without changes as well. When simulation is done locally through LAN cable, simulation is with values without any problem. Any idea what should I check? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/10/2016 3:26:15 PMNew subject after splitting |
|
Follow us on