3/15/2017 5:50 PM | |
Joined: 1/14/2016 Last visit: 10/20/2023 Posts: 4 Rating:
|
Hello everyone I have TIA V13 in VMWARE V11 , and i can't connect with the panel wincc TP1200 confort, i have the configuration network in bridge mode. i have ping with the panel , but when i try go online don´t work. somebody can help me? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/16/2017 2:55:31 PMNew subject after splitting |
|
3/16/2017 8:17 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello eduvega check the basics here: https://support.industry.siemens.com/cs/ww/en/view/58522603 https://support.industry.siemens.com/cs/ww/en/view/88633853 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
3/21/2017 7:46 AM | |
Joined: 1/30/2006 Last visit: 3/17/2025 Posts: 310 Rating:
|
I have had a lot of ethernet / download problems using VW Ware. I bought a USB Ethernet adaptor, did'nt install it in the Host maschine, but only in VM Ware (Attach the hardware). You can find lot of them on ie. Amazon, the shown model is not the one I have That solution have solved all my problems regarding to ethernet communication in VM Ware. BR. -Sven |
BR. Sven |
|
This contribution was helpful to
1 thankful Users |
Follow us on