8/24/2016 4:52 PM | |
Joined: 2/10/2015 Last visit: 6/3/2022 Posts: 245 Rating:
|
I have another concern I have written a HMI project with TIA V13 and I try to transfer it in the display (TP177A), but the transfer does not pass. I transfer with an MPI cable (6ES7 972-0cb20-0xa0) yet I parametered address (3) and the transmission rate (187.5 kbaud) in the display and then after I made a click on transfer and the following message appears: connecting to host now in TIA V13 I made a click on the name of the HMI project and then click on the icon to load in apareil then I chose as MODE in: MPI but I point I can not make a click on load because it is grayed out and I understand nothing, I need your help. thank you ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/25/2016 2:20:42 PMNew subject after splitting |
|
8/25/2016 3:09 PM | |
Joined: 2/10/2015 Last visit: 6/3/2022 Posts: 245 Rating:
|
yes I use a regular laptop with a cable siemens PC USB ADAPTER (6ES7 972-0CB20-0XA0) |
8/25/2016 3:27 PM | |
Joined: 5/12/2006 Last visit: 7/5/2022 Posts: 20616 Rating:
|
Hello, i marked it in you own screen. Regards Christoph |
8/29/2016 11:41 AM | |
Joined: 2/10/2015 Last visit: 6/3/2022 Posts: 245 Rating:
|
Hello thank you, I'll try again |
Follow us on