4/22/2015 2:35 PM | |
Posts: 2 Rating:
|
Hello Everybody I'm testing with the Example Blocks for WinCC (TIA Portal) and STEP 7 (TIA Portal) (for S7-1200 and S7-1500 with SCL)(TIA V13 Pro and WinCC Pro)I use "Tag prefix" for multiplexing and use only one Screen window for all objects.The only PROBLEM that I found, is the Analogue Trend Control, only show the default Data Source that is the first object (example: "Analogue_001.QOUT") and not possible use Tag prefix in this case.Do you recomend me use this Templates ??How can I fixed??Thanks in advance.Regards. |
4/28/2015 9:16 PM | |
Joined: 3/27/2014 Last visit: 4/14/2025 Posts: 5 Rating:
|
Me also having the same issue.
|
4/28/2015 10:45 PM | |
Joined: 3/27/2014 Last visit: 4/14/2025 Posts: 5 Rating:
|
I just make it, by using the vb script for trend control where i put this script at analogue_3 when the picture is open, i attached the project for you to view. Here i attached the file for you to view Attachmentwincc.zip (469 Downloads) |
4/29/2015 10:01 AM | |
Posts: 2 Rating:
|
Very Good idea "sysnergy teo". Thanks I will check. |
Follow us on