6/20/2015 4:39 PM | |
Posts: 33 Rating:
|
Hi Darius , Recently I bought the TIA WinCC Professional SP1 , just because of the C-scripts option , even though the HMI I was configuring was a Comfort Panel . However , I can only use/see the VB scripts . Is there something else that needs to be set in order to enable the C script option ? Regards aney_312
AttachmentCapture_1.zip (201 Downloads) |
Last edited by: Min_Moderator at: 6/22/2015 3:22:09 PMNew subject after splitting |
|
6/23/2015 3:13 PM | |
Posts: 33 Rating:
|
Hi Murof, Thanks. Regards aney_312 |
10/2/2017 12:17 PM | |
Joined: 6/19/2017 Last visit: 12/4/2023 Posts: 7588 Rating:
|
New question published by m.jabbarifar is split to a separate thread with the subject Which package can be used instead of WinCC V7.0 for monitoring with general PCs?. Best regards |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to
1 thankful Users |
7/28/2022 11:13 PM | |
Joined: 2/20/2022 Last visit: 11/5/2023 Posts: 1 Rating:
|
Muito Obrigado |
Follow us on