9/23/2021 3:18 PM | |
Joined: 10/10/2014 Last visit: 8/28/2024 Posts: 1725 Rating: (210) |
Hi makijato Where the project stucked, on zje clinet or from the server ? If the project stuck start the tool rest_wincc.vbs an check if the project run after reset. If not check simatic Shell. How do you use the SIMATIC shell to configure the terminal bus of a WinCC station? https://support.industry.siemens.com/cs/ww/en/view/25437381 With WinCC V7.5 and higher or WinCC Professional V16 and higher how do you activate the setting "Remote Communication" in the SIMATIC shell? https://support.industry.siemens.com/cs/ww/en/view/109769234 Check also the settings according follow FAQ: What settings do you have to make when installing a multiple station system in SIMATIC WinCC Professional? https://support.industry.siemens.com/cs/de/en/view/108464289 Start the tool security control again ! Best regards schufri |
12/9/2022 8:20 AM | |
Joined: 6/16/2022 Last visit: 4/3/2023 Posts: 1 Rating: (0) |
hello; i had the same problem. how did you solve it |
Last edited by: AutoGen_4465708 at: 12/09/2022 08:21:53 |
|