7/2/2013 6:36 PM | |
Posts: 5 Rating:
|
Hello. I have problems communicating with any S7-1200 PLC through TIA V11. The problem began when i forgot to assign the IP ADDRESS to my computer, when i tried searching for the devices it showed me the PLC with the following address (which i assigned) 192.168.0.180, then i tried to communicate with the PLC and the TIA V11 gave me the option of auto assigning the IP ADDRESS to my computer, i clicked YES, since then i wasn't able to communicate with any PLC at all. I tried assigning the IP ADDRESS manually again but that doesn't work anymore. Hope anyone can help me. I attached i file showing what i did and how my computer is reacting now. PS. Sorry if my english is a bit weird or if it is lacking, i'll try my best. English is not my native language. Thanks
AttachmentComm Issue Siemens.zip (130 Downloads) |
7/2/2013 8:10 PM | |
Posts: 5 Rating:
|
Hi,DS SURESH KUMARi don't really get what you are trying to say when you tell me that i have "IP set tool for PLC." The PLC is keeping the IP address, the first picture "Diapositiva01.JPG" is from another computer that actually works communicating. I can see the PLCs in that one. I can also download and upload programs using thatcomputer. With my computer i cannot see the accesibles nodes. I even can't choose my ethernet card. (I already uninstalled the ethernet card and then i reinstalled the driver, still no communication)
|
7/2/2013 11:58 PM | |
Posts: 5 Rating:
|
I also found out this in my computer, in the INFERFACE CONFIGURATION |
Follow us on