9/12/2014 7:54 AM | |
Joined: 11/30/2011 Last visit: 9/4/2024 Posts: 3 Rating: (0) |
At installing TIA13 the installation aborts with the same message.. Can you help me with this? I saw you've been solving this topic more than once.. In attachment you'll find the log files. Kind regards, E. (Barry) Budding
AttachmentSIA_STEP7_PRO_V13@14-09-12_07-44-08.zip (187 Downloads) |
Last edited by: Min_Moderator at: 9/18/2014 3:51 PMDelete E-Mail Last edited by: Min_Moderator at: 9/12/2014 11:21 AMNew subject after splitting from /tf/WW/en/Posts/107097#top |
|
9/15/2014 4:32 PM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello, I recommend to copy the STEP 7 DVD on the hard disc first and after start the installation with the exe file from the hard disk again. Further see the informations of the FAQ in refer to installation rquirements: http://support.automation.siemens.com/WW/view/en/50204569 With best regards |
10/5/2014 11:54 PM | |
Posts: 3 Rating: (0) |
Our upgrade to v13 failed also...did you get your problem resolved?? thx Mike I attached the SIA file & some errors I received....tried the upgrade several times..still fails..not sure if it is a conflict with other software installed on our pc? Unexpected format of the Release Version string: part 2 is not recognized as number - 01 CPR 9 SR 5; Release: 3.51.01 CPR 9 SR 5.1 Setting ExitCode to: 1627 - FunctionFailed 10:22:56|INFO1 |Program::Main() | Exit Main() with global errorcode=1627 Failed to open Windows Installer database: C:\Windows\Installer\36b0f.msi has failed also....any progress on a fix for you yet? AttachmentSIA_STEP7_PRO_V13@14-10-05_09-32-41_AFTERREBOOT_summary.zip (125 Downloads) |
5/24/2016 1:23 PM | |
Posts: 1 Rating: (0) |
hello, i have the same problem, but i think there are more than one error in my logfile... i have admin rights on my pc and started the installation as such after copying the CD to my hard drive. can you help me please? bye AttachmentSIA_STEP7_PRO_V13@16-05-24_13-05-50.zip (73 Downloads) |
Follow us on