4/26/2022 9:32 AM | |
Posts: 34 Rating: (0) |
The situation that i also find myself in is that in TIA17 i cant change the download interface from plcsim to network card. First had a project running which was downloaded to plcsim. Closed this project and plcsim and opened another project that i want to download to a real plc. PG/PC interface is greyed out though and stuck in plcsim. Tried restarting TIA portal with no success. After rebooting pc, pg/pc interface is free again. What need to be done to simplify the possibility to leave plcsim? Meaning being able to change pg/pc interface to something else. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/26/2022 12:55:07New subject after splitting |
|