2/24/2017 4:15 PM | |
Posts: 5 Rating:
|
Dear experts, I am currently wondering if it would be possible to load a recipe (that is, a batch of data records) external to the HMI. As per the topic title, I'm using panel KTP1200 Basic PN (6AV2 123-2MB03-0AX0, version 13.0.1.0) on TIAPortal with WinCC Basic V13 SP 1. I would like to load the data records from an external CSV file. A 1214C DCDCDC PLC is also available, which itself is communicating with the PC where the file is saved. I could load the file indirectly through the PLC, if that is at all possible. As far as I could research, that cannot be done, though. I have read the available documentation, including this document, but nothing seems to have the answer I'm looking for. Thanks and best regards, |
3/2/2017 1:00 PM | |
Posts: 5 Rating:
|
Thanks OpisOm! I was hoping I could integrate the recipes, but I'll look into your suggestion as a workaround. |
Follow us on