3/10/2025 10:52 AM | |
Joined: 1/21/2013 Last visit: 4/18/2025 Posts: 3764 Rating:
|
Hi, The Unified Basic panel does not contain any applications, so Smart Server, which will be the VNC-related application, is not supported. To be honest, to find this information in the technical data, you have to make a comparison between the Unified Basic and the Unified Comfort panel. As far as I know, there are plans to support Smart Server on Unified Basic panels in the future, but I cannot give you any further details. Kind regards |
3/10/2025 11:54 AM | |
Joined: 10/18/2024 Last visit: 3/13/2025 Posts: 21 Rating:
|
I note that Web Client is available on TIAV19 for this HMI. I assume if I enable Web Client on the HMI itself I should be able to login to the HMI using the IP prefixed with https to see the runtime?
|
3/10/2025 11:58 AM | |
Joined: 10/18/2024 Last visit: 3/13/2025 Posts: 21 Rating:
|
Hi Stefan, The web client worked perfectly. Which has solved the problem. Thanks for your help.
|
Follow us on