Industry Online Support
Technical Forum
1/8/2011 10:35 AM | |
Posts: 3 Rating: (0) |
Hai i have to adjust the time and date settings after i switch on the device everytime. Is any possible way to set for once? i have adjusted from HMI suresh |
1/10/2011 7:36 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello How do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible? Best regards, Hristo Mihalev |
1/10/2011 8:10 AM | |
Posts: 3 Rating: (0) |
Sorry i did nt mention that i am using s7200 PLC. |
1/10/2011 8:17 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Don't worry - the story is the same. Just the syntax is a little bit different. How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with WinCC flexible? |