3/30/2009 5:21 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi Sebastian You can do this easy with VBS-script. 1. cycle runnig (1 hour) Create a new action ("File">"New">"Action") and save this action. Klick at the clock in the Toolbar und select the register "Trigger" Klick at the button "Add" Select as Event "Hourly", name the trigger and configure the minute and second of the hour, when the action should run. the number of the hourto set the bit, you get with: bit = DatePart("h", Time) ' the bit mask = 2 ^ bit ' the bit mask At last you need a little bit logic to read and set the value of the variable regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on