7/11/2016 9:27 AM | |
Joined: 4/24/2006 Last visit: 1/13/2025 Posts: 8804 Rating: (1173) |
Hello Paul_NL, Have you seen this: 70011 The system time could not be modified. The error alarm only appears in connection with area pointer "Date/time PLC". Possible causes: •An invalid time was transferred in the job mailbox. •The Windows user has no right to modify the system time. If the first parameter in the system alarm is displayed with the value 13, the second parameter indicates the byte containing the incorrect value. Check the time which is to be set. Possible remedy: Using Windows NT/XP: The user executing WinCC flexible Runtime must be granted the right to change the system time of the operating system. It looks the problem is byte 7. Perhaps this link might help: Clock synchronization between a HMI operator panel and a SIMATIC PLC Best regards, Wizard |
7/11/2016 9:53 PM | |
Posts: 439 Rating: (112) |
Hello, Can you show what DB8 looks like please? Best regards, Hugo |
Last edited by: HugoD at: 7/11/2016 9:54:05 PM |
|
7/11/2016 10:00 PM | |
Posts: 439 Rating: (112) |
Hello Paul, I suppose you already saw this application example, but I don't take chance. Clock synchronization between a HMI operator panel and a SIMATIC PLCBest regards, Hugo |
7/12/2016 8:10 AM | |
Joined: 4/7/2014 Last visit: 6/22/2021 Posts: 40 Rating: (0) |
Hi HugoD, I allready saw that one yes :) Greetings |
7/12/2016 9:02 AM | |
Joined: 4/24/2006 Last visit: 1/13/2025 Posts: 8804 Rating: (1173) |
Hello Paul_NL, What version of TIA Portal are you using? (including updates) Best regards, Wizard |
Follow us on