8/1/2016 4:10 PM | |
Joined: 7/23/2015 Last visit: 5/17/2024 Posts: 26 Rating: (0) |
Hello I want change PLC system time from HMI, I have IO field with time which I want to set to PLC , but when I want change this value , the value doesnt want change and it is only in default value. In system events I have error number 230000. Any idea ? Thank you very much. I add some screens of my program.
AttachmentDokument1.pdf (49 Downloads) |
Last edited by: mirek.kocanda at: 8/1/2016 4:11:43 PM |
|
8/1/2016 4:37 PM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (194) |
Hello mirek.kocanda, I can't help you with the error number, sorry. Did you try to google it? But here are two application examples which are describing your task:
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on