8/31/2016 7:27 AM | |
Joined: 6/13/2010 Last visit: 5/26/2024 Posts: 46 Rating: (3) |
Anyone has idea? |
8/31/2016 9:17 AM | |
Joined: 5/6/2010 Last visit: 1/22/2025 Posts: 2012 Rating: (283) |
Hello jrubio34, if I right understand, you have some varaibles in format TIME and you want to show teh values in a HMI-picture in a resolution 0.1 s? You can show the time with resolution 0.1 s if you scale the value 1:100 (that what you do) and set the decimal places at Properties/general to "1" (see picture 1 at the attachment). Also you can set at Properties/Appearrance/Text/Unit to " s". Then you can see the the s in your I/O-field (see picture 2 at the attachment). I hope this is helpful. regards AttachmentPictures.zip (68 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on