3/27/2015 4:02 AM | |
Joined: 11/12/2006 Last visit: 11/9/2021 Posts: 33 Rating: (0) |
Hi, We have a 6ES7 318-3FL01-0AB0, hardware rev 3, firmware rev 3.2.4. We's just had a very similar problem with timers, following a power failure. Timers that were enabled would never time out. The timer value would just continually cycle around, starting to time down from some meaningless value, above what the timer was set to. Cycling the power didn't help. We resolved this issue by temporarily changing the code to disable the timer, then putting code back the way it should be. I've just had a look though the corrections in the more recent firmware, but I can't find any mention of this issue being fixed. Any sugestions? Regards Ross Umbers Insight Engineering ---------------------------------------------------------------------------------------------------- Split from CPU 317F-2PN/DP timers run and reset without triggers. |
Last edited by: Min_Moderator at: 3/27/2015 8:59:08 AMNew subject after splitting |
|
3/27/2015 4:12 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hello, Have you checked update forV3.2.6 : Update V3.2.6 (6ES7 318-3FL01-0AB0) The above new CPU version does not contain any new functions.
Perhaps, firmware update will help you to solve the problem. I hope these comments help you, Hamid Hosseini |
3/27/2015 4:24 AM | |
Joined: 11/12/2006 Last visit: 11/9/2021 Posts: 33 Rating: (0) |
Thanks, we'll try that. |
Follow us on