11/17/2011 1:49 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Hi, There is many ways to configure an OPC connection between PLC and PC. Here there is a sample of how it could be done. It was used STEP 7 V11 SP1 up2 and SIMATIC NET V7.1 SP2. Follow there is the main steps and, in the sequence, the casts. 1 A – Configure the PLC: IP, IP masc, connect it to a sub network. 1 B – Optional: create symbolic names for tags. 2 A - Configure a PC station with an Ethernet card and OPC. Important: check the version before drag & drop. 2 B – Configure the Ethernet card of the PC. Set the IP, IP masc of the PC. 2 C – Optional: use the symbolic names of the PLC tags. 2 D – Set to export a .XDB file for the PC configuration. 3 - In the Network View configure a interconnection of both Ethernet adapter to the same subnet (by drag and drop). Configure also the S7 connection between OPC and CPU (selecting the connection type and performing a drag and drop). 4 - Compile the PLC HW and download it 5 – Compile the PC HW. 6 and 7 - Copy the .XDB file to a media (e.g. Pen driver) and transport it to the destination PC (where SIMATIC NET will run). 8 – On the target PC, open the Station Configuration Editor and import the XDB file 9 A– For tests proposes, open the OPC Scout (e.g. under START->SIMATIC->SIMATIC NET) 9 B – In OPC Scout , double click on OPC.SimaticNET, give a name for a group (for example, “aaa”). 9C – Open the OPC Navigator, by double click on the created group. 9 D – For absolute address, browser the S7, connection name, Objetcts, M and click on New Definition. For tests proposes, select INT as data type, address 0 and quantity 1. Bring the definition to right side of the window and confirm with ok. Look if the status is showed as “good”. 9 E – Optionally, you can browser symbolic name, brownsing the SYM->Station name-> PLC name. see also the FAQ
"How do you configure an S7 connection for the OPC server of a PC station in STEP 7 (TIA Portal) V11 to access the data of an S7-1200 over Industrial Ethernet?" athttp://support.automation.siemens.com/WW/view/en/3996067 "Data Communication between S7 Station and PC Station, using SIMATIC NET OPC Server" at http://support.automation.siemens.com/WW/view/en/67295801 How do you connect a PC station to an S7-1200 with OPC? |
Last edited by: Pegaia at: 4/8/2013 2:15 PMLast edited by: Pegaia at: 3/25/2013 10:59 AMLast edited by: Pegaia at: 11/15/2012 11:20 PMDenilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
11/17/2011 1:52 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Cast 1a Attachment1a.zip (892 Downloads) |
Denilson Pegaia |
|
11/17/2011 1:58 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Cast 1b
Attachment1b.zip (704 Downloads) |
Last edited by: Pegaia at: 11/17/2011 1:58 PMDenilson Pegaia |
|
11/17/2011 3:54 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Cast 2a Attachment2a.zip (692 Downloads) |
Denilson Pegaia |
|
11/17/2011 3:56 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Cast 2b
Attachment2b.zip (646 Downloads) |
Denilson Pegaia |
|
11/17/2011 4:01 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Cast 2c
Attachment2c.zip (611 Downloads) |
Denilson Pegaia |
|
11/17/2011 4:02 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Cast 2d
Attachment2d.zip (626 Downloads) |
Denilson Pegaia |
|
11/17/2011 4:09 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Cast 3
Attachment3.zip (619 Downloads) |
Denilson Pegaia |
|
11/17/2011 4:12 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Cast 4
Attachment4.zip (604 Downloads) |
Denilson Pegaia |
|
11/17/2011 4:16 PM | |
Joined: 9/23/2005 Last visit: 6/5/2023 Posts: 4184 Rating:
|
Cast 5
Attachment5.zip (618 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
Follow us on