12/27/2017 2:56 PM | |
Joined: 9/23/2005 Last visit: 3/24/2025 Posts: 4406 Rating:
|
Hi, The STEP 7 V15 has a new feature that makes possible to upload an online IO-device configuration to an offline project: Hardware detection of PROFINET IO devices. This feature makes possible timesaving through automatic detection of IO devices, in the cases when there is no exactly information about an IO device during the programming phase or in startup / maintenance, when a real IO device doesn’t match with the project definition (IO device found but showed that the configured device differ of the online device). For the hardware detection of PROFINET IO devices: Requirements:
Procedure (see attached a cast about it)
TIPS: - Detailed information about the procedure could be found in Help -> Show Help ->Information System -> Editing devices and networks -> Configuring devices and networks -> Create configurations -> Configuring PROFINET IO -> Configuring PROFINET IO -> Configure an IO device through hardware detection. - There is no check if a device is already in the project. Every time a device is selected for detection, it is added to project even if it is already in the project. Attachmentv15-1.zip (257 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
4 thankful Users |
Follow us on