12/28/2017 1:16 PM | |
Joined: 9/23/2005 Last visit: 3/14/2025 Posts: 4406 Rating:
|
As from STEP 7 V15 it available a new instruction for ramp generation: RampFunction (Intructions > Technology > PID Control > Auxiliary Functions) The RampFunction block enable to limiting the rate of change and the limit values of a signal with different gradients for positive/ negative/rising/falling signals With this block, it is possible, for example, to generate a ramp for PID set points and so, to get soft and controlled changes of the process variable even with step changes in the original set points. The gradients express how many “unitis” will increase / decrease per second. These gradients could be found in the block instance DB, with the names:
The substitute value input, together with the reset button, could be used to “turn off” the rum function. In the attached example, the same variable was used in the Input and SubstituteOutput inputs. At this way, when Reset = true, the ramp function is deactivated. It should be useful, for example, in the PID tuning phase. The setpoint, gradients and reset are set in WatchTableAttachmentProject1.zip (1022 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
6 thankful Users |
Follow us on