3/1/2013 5:06 PM | |
Joined: 9/23/2005 Last visit: 2/3/2023 Posts: 4178 Rating:
|
Hi, SIMATIC STEP 7 (TIA Portal) V12 TRIAL version is avaliable to download at http://support.automation.siemens.com/WW/view/en/67639464 The enable of the trial license is done by using, when some funtion related is required (for example add a new PLC on a project). TI: In this moment it is necessary to click fist on the license in the wight box and after selected, click on "Activate" buttom. The attached cast show an example how to do it. If the buttom "skip" was pressed, it should be necessary to close the software and restart it again to enable again the "instal trial window. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\TRIAL.zip (1825 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
6/13/2013 11:06 AM | |
Posts: 6 Rating:
|
forgot attachment, excuse |
6/14/2017 11:46 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4839 Rating:
|
New question published by aboali is split to a separate thread with the subject TIA V11, can't open any project or creating one. Best regards |
Follow us on