8/16/2018 3:33 PM | |
Joined: 8/25/2014 Last visit: 4/19/2024 Posts: 133 Rating: (1) |
Hello all. I am trying to communicate with an external device which is ModbusTCP compatible with a S7-1200 PLC. The external device is a heater and I would like to set the setpoint temperature of the heater and periodically check the actual temperature. So I used the example program from Mr.Pegia. When I downloaded the PLC configuration and the PLC code to the PLC I see the following status on the MB_Server block: 7002 - Intermediate call. Connection is being established. This does not change. The command consists of 10 characters, so I sent the following to change the setpoint of the temperature in HEX: 007B, 004D, 0000, 0000, 0000, 0008, 0009, 0008 000D,000A Can anyone please give me some input on what to try next. Cheers. Aleix ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/17/2018 1:03:56 PMInserted splitting-mark. |
|