2/14/2013 8:16 AM | |
Joined: 12/4/2009 Last visit: 12/20/2024 Posts: 453 Rating: (137) |
nicer, some useful stuff for you here and here. There are number of ways how to avoid stop ater download with DB interface changes, but none of them are supported nor recomended. The procedure should not be the same for classic S7 and TIA, since TIA checks consistency prior to any download. Since your IDB has changed it's interface and timestamp, maybe the best way to perform this action is to make brand new FB with fresh IDB's. Download them (and delete the old ones) one by one to avoid memory override. Hope this helps. Best regards. |
Last edited by: crazyCow at: 3/29/2016 1:19:12 PMIf this post actually helped, you may consider using the Rate button above. |
|
This contribution was helpful to3 thankful Users |
Follow us on