Industry Online Support
Technical Forum
11/15/2014 4:32 PM | |
Joined: 5/13/2012 Last visit: 1/17/2024 Posts: 179 Rating: (1) |
dear experts i have a problem when i try to connect my gateway TM 1703 ACP with regional control center. i already connected the SI0 to the national control center and it is OK . but when i try to communicate with SI2 which connected to the regional control center the communication start and appear on the TM 1703 but after two or three second stop ,i don't have any tool to mointer the data between the gateway and SCADA master,but i am using IEC 101 free software as a master and works fine,but when connect the scada the problem happen as i said before. my question is the scada man said that the last event happen to him the there is missmatch address between 2000 address which for data without time tage,and another address 100 with time tage 2-see attached file is it ok to connect the 2,3,5 pin only on RS232 to the Control center. or does i miss something Attachmenthandshake problems.pdf (66 Downloads) |
best regards |
|