2/21/2014 5:11 AM | |
Posts: 7 Rating:
|
Hello , Can any one help me!! Please. I have a project want to read/write data from cpu 315-2dp with TM-1703 via profibus-DP. I have software TBII (vision 5) and sycon (vision 2.6). hardware : TM-1703 with SM-2545 + CM-2869 S7 315-2DP Settings in CPU315-2DP: configure as Profibus-DP Slave Slave address=3 , baud rate= 19.2k , 4 bytes input by unit at slot 4 , 4 bytes output by unit at slot 5 , connect to Master address=2 . Settings in Sycon: BUS baud rate= 19.2k , Optimize = standard . Master = SM-2545 , address = 2 , the others by default . Slave address = 3 , DPV1 actived is check. module insert as follow first ID in general at slot 1 , second ID in general at slot 2 , third ID in general at slot 3, Master_o Slave_i 4 byte by unit at slot 4, Master_i Slave_o 4 byte by unit at slot 5. Settings in TBII : AU = CP 6014 + SM2545/DPM00(install at M PRE 2) But no commnunication between 1703 and 315-2DP. Error message and all settings please check attachment file. Thank you in advence
AttachmentTBII.pdf (143 Downloads) |
2/24/2014 12:26 PM | |
Joined: 8/25/2005 Last visit: 5/25/2023 Posts: 1161 Rating:
|
Hello HSIEH, the Parameter Information send from the DP-Master to the DP-Slave aren't "correct". You got a reply from the Slave. So the Parameters of the Bus should be ok. Maybe you could check the data send at the bus to see more details? For example by using the Amprolyzer Best regards Sabine |
Follow us on