11/17/2018 12:08 AM | |
Posts: 24 Rating: (0) |
Hello all, How do I reset the counter for the card TM PosInput 1? /B |
11/17/2018 12:54 PM | |
Joined: 9/10/2018 Last visit: 5/2/2024 Posts: 17 Rating: (0) |
Can you explain your question well Because the question is so unclear
|
11/18/2018 8:06 PM | |
Posts: 24 Rating: (0) |
Hello, Thanks for the answer. What does "The counter value cannot be influenced by the user program." mean? What are the other ways to reset the counter? /B |
11/18/2018 8:57 PM | |
Posts: 2826 Rating: (685) |
Hello.
If I was in your situation, I would evaluate the example: Thereafter perhaps have a look at the in-software help: BR |
Last edited by: #dP at: 11/18/2018 8:59:48 PM |
|
11/18/2018 10:41 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
You're right, my bad. There's a functional manual that is a must read when using any of the count modules. As #pd noted, have a look at a few examples and if you want more help please specify you hardware, software and what you want to achieve. You can reset Counter Value to equal Start Value in a few ways as per manuals. I have not tried it myself. Examples: "Start value -Reaction to gate start: When the gate is opened, the counter value is set to the start value. -When counting limit is violated: The counter value is set to the start value. -Signal N Synchronization: The configured edge at the respective digital input -Behavior of counter value after Capture:After saving the current counter value as Capture value, counting is continued with the start value. -Stop-Run transition: The technology module is returned to its startup state after a
|
11/18/2018 10:49 PM | |
Posts: 24 Rating: (0) |
Thanks for taking the time. I will check the SW gate if it works. /B |
Follow us on