4/7/2022 6:20 AM | |
Joined: 6/11/2021 Last visit: 3/21/2025 Posts: 4 Rating:
|
Good morning, I am trying to connect to the drive via Data Block and so far I am unable to control the axis using MC motion commands or via Axis Control Panel inside the TO Commissioning. Project Info:
There are no errors or alarms in my PLC or Drive currently and, I am at a lost of what are the next steps: What have I done so far:
In the PLC diagnostics buffer I get the following description: MC alarm 421: Drive under logical address 0 faulty. Alarm message from drive. MC component: PositioningAxis_1, TO_DB= 1 Outgoing event: No user action required In the Drive I see this message at the operating display: Switching on inhibited - set "OC/OFF2" = "1" It looks to me that there is some mapping issue but cannot find why as the IO addresses in the drive config are used for the PLC Tags. There is little information regarding this topic, so far I have read the manuals: 109741575 and A5E03879256-AE but found very little info on programming inside the MC PreServo and MC PostServo OBs. Any help would be greatly appreciated Thank you, Mr_Motion
AttachmentDiagnostics_TEL3.txt (711 Downloads) |
Last edited by: Mr_Motion at: 04/07/2022 06:50:09 |
|
4/7/2022 1:42 PM | |
Joined: 9/23/2005 Last visit: 3/21/2025 Posts: 4965 Rating:
|
How about this application example ? |
Regards, |
|
4/11/2022 2:09 PM | |
Joined: 11/4/2011 Last visit: 3/21/2025 Posts: 263 Rating:
|
Hi there, you cannot write these parameters from the user program. See here, column W: https://support.industry.siemens.com/cs/de/en/view/109781849/132833072523 And for the meaning of the values in column W see here: https://support.industry.siemens.com/cs/de/en/view/109781849/118974587915 But anyway, what's the sense in writing some of the most basic configuration parameters of the TO during runtime? Why? Regards, |
Follow us on