4/2/2017 3:26 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Hi all, Do anyone know how to create a c script/ vb / dynamic dialog / direct connection to copy tagprefix of Picture Window to an picture object "static text' ? For example, the object in the picture window having the dynamic link of ".value". (dynamic) There is one property of the object named "tagname". (static) If the tag prefix of the picture window is "Valve1/Ctrl" , i want the static "tagname" to copy this tag prefix and output as "Valve1/Ctrl" Hope my question is clear. Anyone know how to do this? Thanks for helps. *PCS 7 V8.2, WinCC V7.4. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
4/5/2017 1:27 PM | |
Joined: 3/13/2015 Last visit: 4/29/2024 Posts: 122 Rating: (38) |
Hi, Harry's suggestion is possible. If it is necessary to derive the information from the tag:
See for more information about this function and the structure linkinfo: Regards, |