11/26/2012 12:53 PM | |
Joined: 7/17/2012 Last visit: 3/3/2025 Posts: 42 Rating:
|
Hi, I have problem with simulation TP1200 Comfort Panel. My notebook resolution is 1280x800 and the same resolution is on the panel, but when I turn on simulation, the resolution is much larger.I have to use sliders, it's so annoying. How to change it? |
Last edited by: majklkl at: 11/26/2012 12:53 PM |
|
11/26/2012 3:04 PM | |
Posts: 3037 Rating:
|
Hello, you can not change the panel resolution of TP1200 Comfort. You can use the WinCC advanced Runtime with 1280*800, then you have not the layout of TP1200 Comfort. Tweety |
12/13/2012 9:50 PM | |
Posts: 11 Rating:
|
can you grab the corner of the runtime simulation windows with the double arrow <--> cursor and drag it in to fit your screen? I can adjust the size of a KTP600 this way. |
12/14/2012 6:40 AM | |
Joined: 8/31/2010 Last visit: 2/8/2025 Posts: 1524 Rating:
|
Hello maynyrd, Increase the resolution of your laptop / PC, so that you can accommodate the screen size. Or else as you say you can resize it also. |
Like it? Rate it! |
|
Follow us on