2/5/2021 9:53 AM | |
Joined: 6/30/2017 Last visit: 10/22/2024 Posts: 7 Rating: (0) |
Hi, I have problems to implement the computed torque control library , I have following the manual but when I enable the IdentifyTorqueControl the CPU go to stop and I dont know why. I attached my code implemented in Pre-Servo, because I think that is there the problem. In the library has the get_dynamics function for two times, but the second time before de calc torques are in comments because if I put it the cpu go to stop too.
AttachmentPreservo.txt (334 Downloads) |
Last edited by: LowClue at: 02/05/2021 09:55:49Last edited by: LowClue at: 02/05/2021 09:56:01Last edited by: LowClue at: 02/05/2021 09:56:56Last edited by: LowClue at: 02/05/2021 09:57:42 |
|
2/5/2021 9:54 AM | |
Joined: 6/30/2017 Last visit: 10/22/2024 Posts: 7 Rating: (0) |
In the buffer error. |
Follow us on