10/1/2008 5:01 PM | |
Joined: 9/18/2006 Last visit: 2/6/2024 Posts: 589 Rating: (64) |
Hi. Example in SINAMICS S120 Function Manual, 03/2006 Edition. The drive first generates torque against the applied brake. The brake is not released until the motor torque or motor current (p1220) has exceeded braking threshold 1 (p1221). This configuration is used, for example, when the drive is connected to a belt that is under tension (loop accumulator in the steel industry). Successes. AttachmentExample Brake.pdf (208 Downloads) |
Follow us on