5/31/2016 11:01 AM | |
Joined: 6/23/2015 Last visit: 8/4/2022 Posts: 1 Rating:
|
Hello, I have some trouble with the setting to desabled the touch beep. My sounds seeting is Off ( as I want it to be) When I start the Application, sounds are off . But when I put the KTP700's supply off and on, touch beep are in function again while the setting is still OFF . I have 2 KTP700 and both do the same. Thanks to help me. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/31/2016 2:07:26 PMNew subject after splitting |
|
Follow us on