9/20/2020 2:54 PM | |
Posts: 8 Rating:
|
Hi, I am using the same HMI panel and I am trying to figure out which interface I have to use. The physical part of the interface is obvious but I am not sure about the protocol. Is it ISO or TCP? Edit: I still have the problem, but found an answer to my question regarding the protocol. It should be TCP (documentation in this regard) I attached a picture of the error for both of them. The result is the same in both cases, the simulated HMI can't read out parameters and cannot change them either. When I upload the same program to the real HMI, it works perfectly. Extra question: Is it possible to run the simulation in the regular WinCC, instead of the advanced one? I have only a trial license for the advanced one, and I thought maybe that is the source of the problem somehow. ------------------------------------------------------------------------------------------ |
Last edited by: balint at: 09/20/2020 15:05:49Last edited by: The Helping Hand at: 09/23/2020 09:40:20New subject after splitting |
|
9/21/2020 2:09 PM | |
Joined: 5/12/2006 Last visit: 4/24/2025 Posts: 22624 Rating:
|
which ip settings you use on the PC? |
This contribution was helpful to
1 thankful Users |
Follow us on