1/11/2018 8:29 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, please have a look: http://support.automation.siemens.com/WW/view/en/19109408 you can use RS232/PPI multimaster cable or USB/PPI multimaster cable for both |
This contribution was helpful to
1 thankful Users |
1/11/2018 5:39 PM | |
Joined: 9/21/2012 Last visit: 3/19/2025 Posts: 4331 Rating:
|
I would buy this: PC Adapter USB A2 |
Last edited by: Jen_Moderator at: 1/15/2018 12:57:54 PMInserted right link. |
|
1/13/2018 2:44 PM | |
Posts: 8946 Rating:
|
It seems that you are a great fan of "PC Adapter USB A2". |
1/18/2018 4:20 PM | |
Joined: 8/3/2009 Last visit: 3/19/2025 Posts: 15022 Rating:
|
Hello Be careful with this strange TP177A its a special unit. -> If you load the first Time you just can load with MPI or PPI -> If you then load a Project with a PROFIBUS Connection configuration then you also can use the DP Transfer and Communication If would use a CP like CP5711 with is you should have no Problems. BUt if you look here: https://support.industry.siemens.com/cs/de/en/view/19109408 The PC Adapter USB is also suitable for this special Panel... Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on