11/8/2010 8:45 PM | |
Joined: 3/21/2006 Last visit: 3/17/2025 Posts: 10239 Rating:
|
Hello, Let's start with manual concerning 7ML52211-BA21. BR, Hristo Mihalev |
11/9/2010 12:04 PM | |
Joined: 3/21/2006 Last visit: 3/17/2025 Posts: 10239 Rating:
|
Hello again, CPU314C-2DP 1. MPI connection on port 1 with TP170A 2. Profibus connection on port 2 with sonic sonar. For both connection you will need connectors like in Product Information on PROFIBUS-bus connector with/without PG socket to 12 MBaud To be possible to connect PG to the port 1 (MPI connection) you will need to chose there Profibus connector with PG socket. Of course there will be use Profibus cable like 6XV1830-0AT15LAN CABLE PROFIBUS 150 M (you could use any manufactures which cover the profibus standards). For the connection between PG and CPU you will need for example - 6ES7972-0CB20-0XA0SIMATIC S7, PC ADAPTER USB Of course there is possible another ways and using another hardware... Hope this helps. Best regards, Hristo Mihalev |
11/9/2010 8:20 PM | |
Posts: 11 Rating:
|
i saw the adabter ....does it mean that 1 (9 pins) end to the dp port in the plc ....other one for PC and the 2 cables for i/o devices ??? am i right ?? |
Follow us on