11/27/2017 4:41 PM | |
Posts: 14 Rating:
|
Hi, I would like to ask is that any options that allows end-user to choose the points to show on the trending views on TP 1200? Thank You. |
11/28/2017 1:21 PM | |
Posts: 648 Rating:
|
Hey 86988, you can use the "WinCC Trend Control". Go through the "properties" of the control. Activate the toolbar under "Properties > Toolbar" (screenshot3). If the runtime is running you can stop the current trend with the toolbar and use the lineal to read the choosen data set (screenshot1). With best regards rh1990 AttachmentScreenshots.zip (85 Downloads) |
11/30/2017 11:12 AM | |
Posts: 648 Rating:
|
Hey 86988, this functionality is not implemented in the WinCC Trend Control for WinCC RT Advanced. With best regards rh1990 |
Follow us on