Industry Online Support
Technical Forum
10/22/2014 4:25 PM | |
Posts: 1058 Rating:
|
Hello philhoward, the TP1200 is operated with Windows CE 6.0 operating system, so actually that will set the limits for operable volumes. So I hope you will find your answers here: Maximum supported Memory Card & File Sizes under Windows CE This article discusses the file system driver limitations of Windows CE FAT12/FAT16/FAT32 implementation. It outlines the maximum supported and maximum recommended peripheral memory devices under Windows CE, including Compact Flash (CF), SD, MMC, ATA Flash, USB memory fobs and external hard drives. regards |
10/23/2014 8:41 AM | |
Posts: 4 Rating:
|
Many thanks - looks like no reaslistic restriction then! |
Follow us on