9/27/2017 10:19 AM | |
Joined: 6/29/2017 Last visit: 1/31/2025 Posts: 4 Rating:
|
Hello, All. My TP1500 stay in loading boot(lsimatic's logo) and not start Windows. I didn't made any updates etc. And Ethernet connectors everytime lit even without connection. Have you an idea, what can be the reason of this. How to fix it. Thank you. |
This contribution was helpful to
1 thankful Users |
9/27/2017 11:06 AM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello, It looks like the image is not well. Please try to preform an OS update, with the option 'Reset to factory settings selected': Best regards, Wizard |
9/27/2017 12:44 PM | |
Joined: 6/29/2017 Last visit: 1/31/2025 Posts: 4 Rating:
|
Thank you for answer. But I can not connect to HMI. Profinet X1 connectors are lit (also without any connection) and Profinet connector X3 does not lit (even with connection). And there is not ping from my PC to HMI |
9/27/2017 1:31 PM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello, Try to use the description using Prosave. When you 'reset to factory settings', you will have to Boot panel. Then communication will use MAC adres to communicate (No ip-adres) Best regards, Wizard |
9/27/2017 1:58 PM | |
Joined: 6/29/2017 Last visit: 1/31/2025 Posts: 4 Rating:
|
I tried to make this. I did enter MAC-address and IP-address. I've got message that connection established. I've got ProSave window, I've pressed "Yes", got suggection to boot HMI and nothing more happens. |
9/27/2017 2:26 PM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello, I guess you boot the panel? But nothing happens. When you panel boots, Prosave is trying to communicate using the MAC adress, perhaps a Virusscanner or Firewall is blocking this communication. Best regards, Wizard |
10/23/2019 10:25 AM | |
Joined: 2/10/2015 Last visit: 2/26/2025 Posts: 1 Rating:
|
In this case, I think we write OS.image file to Flash Memory number AT25DF321A should be able to do but requires special tools Is a read-write EEPROM I use this model TP1500 Comport 8 pcs. and encounter problems like yours too Which I am trying to write EEPROM If effective, will update again. |
10/28/2019 10:01 PM | |
Joined: 4/21/2015 Last visit: 11/17/2024 Posts: 56 Rating:
|
hi I read eeprom from a panel correct & write to eeprom but stuck at simatic hmi yet
|
6/23/2021 4:02 PM | |
Joined: 2/12/2021 Last visit: 12/3/2024 Posts: 5 Rating:
|
Hi Slawek / Murof, I am facing the very same issue. Any progress on this thread? Did you manage to solve it ? Best regards, |
10/19/2022 11:44 AM | |
Joined: 2/12/2021 Last visit: 12/3/2024 Posts: 5 Rating:
|
Just feeding back on the post, my issue was exactly as mentioned by Murof. Activities were being blocked by the company Firewall. It took a bit longer to have visibility on this as it was a global application. Thanks! |
This contribution was helpful to
1 thankful Users |
10/28/2022 11:54 AM | |
Joined: 8/3/2009 Last visit: 3/14/2025 Posts: 14990 Rating:
|
Hello This is always a problem that you often will not be able to clear by yourself. The only thing is to try a reset to factory settings. If this not work... I this case send the Panel to Siemens Repait Center. Murof |
If this Information really helps, you could use the Rate function |
|
12/14/2022 12:29 PM | |
Joined: 10/7/2021 Last visit: 12/4/2024 Posts: 1 Rating:
|
Hi, I have encountered the same problem as you, have you solved this problem, I hope to get your reply, thank you very much |
9/2/2024 9:12 AM | |
Joined: 3/15/2021 Last visit: 10/8/2024 Posts: 1 Rating:
|
Hi, I used Brain's advice, changed PG/PC Settings and was able to reset to factory settings. https://support.industry.siemens.com/forum/WW/en/posts/tp700-comfort-the-os-does-not-boot/168455?page=2 |
Follow us on