3/16/2014 10:37 AM | |
Posts: 26 Rating:
|
1 I'm not able to communicate via PC Adapter usb. I tried all options and it didnt work 4 I found two versions of rs232/null modem cable.Which one is appropiate? greetings Attachmentrs232 (2).zip (185 Downloads) |
3/16/2014 4:31 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hi gregory24, 1-How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this? 4-Take a look: TP170A communication problem |
3/17/2014 8:39 AM | |
Joined: 4/24/2006 Last visit: 4/23/2025 Posts: 8965 Rating:
|
Hello gregory24, Perhaps the following links might help: Which connector cables are available for connecting to SIMATIC Panels? how can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Best regards, Wizard |
Follow us on