7/24/2018 10:52 AM | |
Posts: 2 Rating:
|
Good Morning, Please could someone assist me with some information regarding the TP170B. I don't have the original project file for this TP so I would like to be as careful as possible I have made a Complete Backup in ProSave v6.0, the Panel is currently running OS v6.0. If i update this panel to OS v7.2 will my backup that I made .psb still work? If I download something to it from WinCC Flex 2008 after I update to v7.2, will I still be able to restore the v6.0 .psb backup file using ProSave if something goes wrong even though the OS will then be at v7.2? Thanks in advance! Nic |
7/30/2018 3:49 PM | |
Joined: 8/3/2009 Last visit: 3/14/2025 Posts: 14990 Rating:
|
Hello NicholasR No this won´t work because the Backup with Prosave or to Storagecard includes also the Operating System -> so its a complete Image of the Panel. IF you restore it to the Panel then everything will be overwritten, also the Operation System and the Settings and so on. If you so not have the Project file you can only make several Backups, try to get an equal Spare Part Device and pray that the Panel works future. Without the Project you can not do anything.... Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |